I am trying to implement two LAN ports by attaching a Gigabit Ethernet Switch IC (KSZ9567R or KSZ9563R) to i.MX6Q. But I can not see the product I implemented. Is this a problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am trying to implement two LAN ports by attaching a Gigabit Ethernet Switch IC (KSZ9567R or KSZ9563R) to i.MX6Q. But I can not see the product I implemented. Is this a problem?

724 Views
yuoncheulna
Contributor I

i.MX6Q + Gigabit Ethernet Switch IC(KSZ9567R or KSZ9563R)

Labels (1)
0 Kudos
1 Reply

431 Views
igorpadykov
NXP Employee
NXP Employee

Hi YUONCHEUL

you are right nxp bsps described below do not support that chip

i.MX Software|NXP 

One can look at efforts on below link with similar product

https://community.nxp.com/thread/463677 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos