CPU: Freescale i.MX53 family 2.1V at 800 MHz
mx53 pll1: 800MHz
mx53 pll2: 400MHz
mx53 pll3: 216MHz
mx53 pll4: 455MHz
ipg clock : 66666666Hz
ipg per clock : 33333333Hz
uart clock : 66666666Hz
cspi clock : 54000000Hz
ahb clock : 133333333Hz
axi_a clock : 400000000Hz
axi_b clock : 200000000Hz
emi_slow clock: 133333333Hz
ddr clock : 400000000Hz
esdhc1 clock : 80000000Hz
esdhc2 clock : 80000000Hz
esdhc3 clock : 80000000Hz
esdhc4 clock : 80000000Hz
nfc clock : 26666666Hz
Board: MX53-LOCO 1.0
Boot Reason: [POR]
Boot Device: SD
I2C: ready
DRAM: 1 GB
MMC: FSL_ESDHC: 0, FSL_ESDHC: 1
*** Warning - bad CRC or MMC, using default environment
IPU CLK = 200000000
MXC IPUV3 configured
XRES = 320 YRES = 240 BitsXpixel = 4
In: serial
Out: serial
Err: serial
Serial reinitilized!
Net: got MAC address from IIM: 00:04:9f:02:41:18
FEC0 [PRIME]
Hit any key to stop autoboot: 0
MX53-LOCO U-Boot >
MX53-LOCO U-Boot >
MX53-LOCO U-Boot > usb start
(Re)start USB...
USB: Register 10011 NbrPorts 1
USB EHCI 1.00
scanning bus for devices... New Device 0
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x100 index 0x0 length 0x40
USB DESCRIPTOR 18
set address 1
usb_control_msg: request: 0x5, requesttype: 0x0, value 0x1 index 0x0 length 0x0
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x100 index 0x0 length 0x12
Sar - New Device Max Ports are: 0
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x200 index 0x0 length 0x9
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x200 index 0x0 length 0x19
get_conf_no 0 Result 25, wLength 25
if 0, ep 0
##EP epmaxpacketin[1] = 8
set configuration 1
usb_control_msg: request: 0x9, requesttype: 0x0, value 0x1 index 0x0 length 0x0
new device strings: Mfr=1, Product=2, SerialNumber=0
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x300 index 0x0 length 0xFF
USB device number 1 default language ID 0x1
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x301 index 0x1 length 0xFF
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x302 index 0x1 length 0xFF
Manufacturer u-boot
Product EHCI Host Controller
SerialNumber
USB hub found
usb_control_msg: request: 0x6, requesttype: 0xA0, value 0x2900 index 0x0 length 0x4
usb_control_msg: request: 0x6, requesttype: 0xA0, value 0x2900 index 0x0 length 0x8
1 ports detected
individual port power switching
standalone hub
global over-current protection
power on to power good time: 20ms
hub controller current requirement: 0mA
port 1 is removable
usb_control_msg: request: 0x0, requesttype: 0xA0, value 0x0 index 0x0 length 0x4
get_hub_status returned status 1, change 8101
local power source is lost (inactive)
no over-current condition exists
enabling power on all ports
usb_control_msg: request: 0x3, requesttype: 0x23, value 0x8 index 0x1 length 0x0
port 1 returns 0
usb_control_msg: request: 0x0, requesttype: 0xA3, value 0x0 index 0x1 length 0x4
Port 1 Status 301 Change 1
port 1 connection change
port 1 connection change
usb_control_msg: request: 0x0, requesttype: 0xA3, value 0x0 index 0x1 length 0x4
portstatus 301, change 1, 1.5 Mb/s
usb_control_msg: request: 0x1, requesttype: 0x23, value 0x10 index 0x1 length 0x0
hub_port_reset: resetting port 0...
usb_control_msg: request: 0x3, requesttype: 0x23, value 0x4 index 0x1 length 0x0
usb_control_msg: request: 0x0, requesttype: 0xA3, value 0x0 index 0x1 length 0x4
portstatus 303, change 10, 1.5 Mb/s
STAT_C_CONNECTION = 0 STAT_CONNECTION = 1 USB_PORT_STAT_ENABLE 1
usb_control_msg: request: 0x1, requesttype: 0x23, value 0x14 index 0x1 length 0x0
New Device 1
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x100 index 0x0 length 0x40
EHCI timed out on TD - token=0x80008c80
USB DESCRIPTOR 64
hub_port_reset: resetting port 0...
usb_control_msg: request: 0x3, requesttype: 0x23, value 0x4 index 0x1 length 0x0
usb_control_msg: request: 0x0, requesttype: 0xA3, value 0x0 index 0x1 length 0x4
portstatus 303, change 10, 1.5 Mb/s
STAT_C_CONNECTION = 0 STAT_CONNECTION = 1 USB_PORT_STAT_ENABLE 1
usb_control_msg: request: 0x1, requesttype: 0x23, value 0x14 index 0x1 length 0x0
set address 2
usb_control_msg: request: 0x5, requesttype: 0x0, value 0x2 index 0x0 length 0x0
EHCI timed out on TD - token=0x80008d80
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x100 index 0x0 length 0x12
EHCI timed out on TD - token=0x80008c80
Sar - New Device Max Ports are: 0
USB GET DESCRIPTOR
usb_control_msg: request: 0x6, requesttype: 0x80, value 0x200 index 0x0 length 0x9
EHCI timed out on TD - token=0x80008c80
usb_get_configuration_no: failed to get descriptor - too long: 65535
ERROR: NOT USB_CONFIG_DESC ff
set configuration 0
usb_control_msg: request: 0x9, requesttype: 0x0, value 0x0 index 0x0 length 0x0
EHCI timed out on TD - token=0x80008d80
new device strings: Mfr=0, Product=0, SerialNumber=0
Manufacturer
Product
SerialNumber
Manufacturer
Product
SerialNumber
2 USB Device(s) found
scanning bus for storage devices...
0 Storage Device(s) found
解決済! 解決策の投稿を見る。
Hi friend,haven‘t you solve this problem.Can you share the ehci_mx5.c file?
Thanks very much.:smileyhappy:
Yes, correct. On mx53qsb USBHost works by default on the latest U-boot.
Hi Fabio Estevam
I found a problem when i debug,now this is my print
CPU: Freescale i.MX53 family 2.1V at 800 MHz
mx53 pll1: 800MHz
mx53 pll2: 400MHz
mx53 pll3: 432MHz ------------------------------this is important
mx53 pll4: 455MHz
ipg clock : 66666666Hz
ipg per clock : 33333333Hz
uart clock : 66666666Hz
cspi clock : 108000000Hz-------------------and this
ahb clock : 133333333Hz
axi_a clock : 400000000Hz
axi_b clock : 200000000Hz
emi_slow clock: 133333333Hz
ddr clock : 400000000Hz
esdhc1 clock : 80000000Hz
esdhc2 clock : 80000000Hz
esdhc3 clock : 80000000Hz
esdhc4 clock : 80000000Hz
nfc clock : 26666666Hz
Board: MX53-LOCO 1.0
Boot Reason: [POR]
Boot Device: SD
but the iMX53RM write the usbhost working on the PLL3 216mhz,setup_pll PLL3_BASE_ADDR,216 is writen
in the lowlevel_init.S, Why it become 432MHZ,and what should i do to change it to 216mhz ,I used u-boot-2009.08
thanks!
yang rui
Please use 2013.01. U-boot instead. You will get USB Host working out of the box.
Hi Fabio,
but the u-boot 2013.04 has not mxc_nand_bi_swap function in driver/mtd/nand/mxc_nand.c file, so the NAND flash bad block management is not correctly managed and it can be cause some malfunctions with the NAND.
Or perhaps the bad block indicator swap is now implemented in another way?
Flavio
Flavio,
This thread is about usb host support in U-boot for mx53, not about NAND.
ok
Well i am using the freescale's MX53-Start-R board for the same. I am trying to recognise the USB Mass storage through USB Host1.
I am also attaching the mx53_loco.h file in which i have include the following for USB:
#define CONFIG_CMD_USB
#define CONFIG_USB_EHCI
#define CONFIG_USB_EHCI_MX5
#define CONFIG_USB_STORAGE
#define CONFIG_USB_HOST_ETHER
#define CONFIG_USB_ETHER_ASIX
#define CONFIG_USB_ETHER_SMSC95XX
#define CONFIG_MXC_USB_PORT 1
#define CONFIG_MXC_USB_PORTSC (PORT_PTS_UTMI | PORT_PTS_PTW)
//#define CONFIG_MXC_USB_FLAGS (1 << 5)
#define CONFIG_MXC_USB_FLAGS 0
#define CONFIG_MX53
#define CONFIG_EHCI_HCD_INIT_AFTER_RESET
#define CONFIG_EHCI_IS_TDI
#define CONFIG_SUPPORT_VFAT
| #define CONFIG_CMD_FAT | 1 |
Am I missing something??
Please suggest...