I am having problems with image files for CL-SOM-iMX7

cancel
Showing results for 
Search instead for 
Did you mean: 

I am having problems with image files for CL-SOM-iMX7

184 Views
aaronpadilla
Contributor II


Hi there,

 

I am trying to boot the board following the document:

 

CL-SOM-iMX7: Linux: Getting started - CompuLab Wiki

I have tried the auto-installation and the manual installation but I am always getting a problem with the root fs.

 

Could you advice?

Thanks

Original Attachment has been moved to: log_imx7.txt.zip

0 Kudos
1 Reply

84 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Aaron

seems root parameter (like "setenv bootargs 'root=/dev/ram0 ramdisk_size=16384")

in kernel command line was not provided.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos