I.Mx 233 can boot from 4k page size nand ( 4096 + 224 bytes)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.Mx 233 can boot from 4k page size nand ( 4096 + 224 bytes)

700 Views
kishorepoojari
Contributor III

Hello All,

   Can I.Mx 233  boot from 4k page size Nand ( 4096 + 224 bytes).

Regards,

Kishore P

Labels (1)
Tags (5)
0 Kudos
3 Replies

414 Views
igorpadykov
NXP Employee
NXP Employee

Hi kishore

yes it can in theory, though seems this was not tested.

However NAND ecc requirement should be <= 20 bit (max. BCH value).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

414 Views
kishorepoojari
Contributor III

Hi igor,

   I have set CHIP_BCB_SECTOR_STRIDE to 128 , CHIP_BCB_BLOCK_LIMIT to 4 and ecc to 4 , The NCB , LDLB and DBBT information are correctly written to Nand. But If I boot through Nand following error thrown by ROM code 0x80508003 Unable to find LDLB.

Regards,

Kishore P

0 Kudos

414 Views
igorpadykov
NXP Employee
NXP Employee

Hi kishore

answer is given on link

https://community.freescale.com/thread/340078

Best regards

igor

0 Kudos