I.MX9352 M33 Problems with output floating-point data when developing with IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX9352 M33 Problems with output floating-point data when developing with IAR

947 次查看
HL_G
Contributor II

Hello.

When developing I.MX9352 Cortex-M33 with IAR1 9.50.2, it was not possible to output floating-point data via redirected printf.

The SDK used is SDK_2_16_000_MIMX9352xxxxM

The following Settings have been made in the IAR Settings.

HL_G_0-1729821245424.png

 

Here's my code:

/*
 * Copyright (c) 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_debug_console.h"
#include "fsl_rgpio.h"

/*******************************************************************************
 * Definitions
 ******************************************************************************/
#define BOARD_LED_RGPIO          GPIO3
#define BOARD_LED_RGPIO_PIN      26U
#define EXAMPLE_RGPIO_CLOCK_ROOT kCLOCK_Root_BusWakeup
#define EXAMPLE_RGPIO_CLOCK_GATE kCLOCK_Gpio3
double Pi = 3.1415926;

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
/*!
 * @brief delay a while.
 */
void delay(void);

/*******************************************************************************
 * Variables
 ******************************************************************************/

/*******************************************************************************
 * Code
 ******************************************************************************/

/*!
 * @brief Main function
 */
int main(void)
{
    /* Define the init structure for the output LED pin*/
    rgpio_pin_config_t led_config = {
        kRGPIO_DigitalOutput,
        0,
    };

    /* Board pin, clock, debug console init */
    /* clang-format off */

    const clock_root_config_t rgpioClkCfg = {
        .clockOff = false,
        .mux = 0, // 24Mhz Mcore root buswake clock
        .div = 1
    };
    /* clang-format on */
    BOARD_InitBootPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    CLOCK_SetRootClock(EXAMPLE_RGPIO_CLOCK_ROOT, &rgpioClkCfg);
    CLOCK_EnableClock(EXAMPLE_RGPIO_CLOCK_GATE);
    CLOCK_EnableClock(kCLOCK_Gpio2);
    /* Set PCNS register value to 0x0 to prepare the RGPIO initialization */
    BOARD_LED_RGPIO->PCNS = 0x0;

    /* Print a note to terminal. */
    PRINTF("\r\n RGPIO Driver example\r\n");
    PRINTF("\r\n The LED is taking turns to shine.\r\n");

    /* Init output LED GPIO. */
    RGPIO_PinInit(BOARD_LED_RGPIO, BOARD_LED_RGPIO_PIN, &led_config);

    while (1)
    {
      
      PRINTF("output float value:Pi=%f %lf\r\n", Pi, Pi);
        SDK_DelayAtLeastUs(1000000U, SystemCoreClock);
        RGPIO_PortToggle(BOARD_LED_RGPIO, 1u << BOARD_LED_RGPIO_PIN);
    }
}

The actual effect is as follows:

HL_G_1-1729821805873.png

 

 

标记 (1)
0 项奖励
回复
3 回复数

905 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @HL_G 
Please refer this case to modify PRINTF function in SDK:

https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Cannot-print-float-values-from-SDK-M7-examples/...

Best Regards
Zhiming

0 项奖励
回复

895 次查看
HL_G
Contributor II

Hi.@Zhiming_Liu
Thanks.
It seems that this approach is no better than using the sprintf function to convert to string output. Is there a way to print floating-point data directly using PRINTF?
Like this:

main()
{
double pi = 3.1415926;
PRINTF("pi = %f\r\n", pi);
}

The output:

pi = 3.141593
0 项奖励
回复

890 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello,

The existing PRINTF has a bit of a problem with float, or if you're not using serial printing and use printf inside the IAR

Best Regards,
Zhiming

0 项奖励
回复