Hi NXP,
I try to use uuu-tool and "LF_v5.15.52-2.1.0_images_IMX8ULPEVK" for burn iMX8ULP demo image.
But I got below SPL log. How can I solve this problem ?
My steps :
1. Change SW5 to "01xx_xxxx"
2. Power on the EVK to enter USB download mode.
3. run "sudo ./uuu -b emmc imx-boot-imx8ulp-9x9-lpddr4-evk-sd.bin-flash_singleboot"
U-Boot SPL 2022.04-lf_v2022.04+g16e8414193 (Oct 08 2022 - 13:33:43 +0000)
Normal Boot
ELE firmware version 0.0.7-c62a7493
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.6
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.14
Turn on switches ok
Turn on memories ok
Clear DDR retention ok
Enable AFBB for APD bias ok
SEC0: RNG instantiated
Trying to boot from BOOTROM
Boot Stage: USB boot
Can't found uboot image in 640K range
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###