I.MX8QMAX : bitbake fsl-image-qt5-validation-imx -c populate_sdk Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8QMAX : bitbake fsl-image-qt5-validation-imx -c populate_sdk Error

1,229 Views
santhosh2
Contributor IV

Hi,

I have got below error when doing bitbake fsl-image-qt5-validation-imx -c populate_sdk


Computing transaction...error: Can't install packagegroup-core-ssh-dropbear-1.0-r1@all: it's locked


Please find the snap shot attached

populate_sdk.png

Let me know how to resolve this


Regards

Santhosh

0 Kudos
Reply
2 Replies

1,120 Views
santhosh2
Contributor IV

Hi,

after comminting the below packages in local.conf file I am getting the error(please ref the screen shot)

#SSH
#PACKAGE_EXCLUDE += " packagegroup-core-ssh-dropbear"
#CORE_IMAGE_EXTRA_INSTALL += "openssh"

populate_sdk1.png

I tried below

bitbake -f fsl-image-qt5-validation-imx

bitbake fsl-image-qt5-validation-imx  -c populate_sdk

but still get the above error

Regards

Santhosh

0 Kudos
Reply

1,120 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Santhosh Kumar, 

I'd like to try to reproduce this error. I would like to confirm the BSP you are using, is it the L4.9.51 BSP? Is it the GA or the Beta version? If it's the later it would make sense to switch to the GA in case this error was corrected. And also, are you following the Yocto Project User's Guide? Would you please share the setting (Distro, Machine) you are using?


Regards,

0 Kudos
Reply