[I.MX8MQ-EVK] for secure boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[I.MX8MQ-EVK] for secure boot.

433 Views
Ashoka_A_D
Contributor I

Hi All,

I have i.mx8mq-evk board, i want to start the secure boot in it. any body can help me to do this from scratch.? 

i have  few doubts.

1. can i able to do the secure boot in this board.?

2. Is OTP is present on the board.?

 

Advance thanks for your response.

0 Kudos
2 Replies

417 Views
frix
Contributor II

Just a heads up - if you proceed to encrypted boot, there's a typo in mx8m_encrypted_boot.txt:

Line 454:   MAC offset = csf_fit_enc.bin size - Nonce/MAC size
Line 455:                      = 4020 - 36 = 3984 Byte

The file referenced, should be 'csf_fit_sign_enc.txt', not 'csf_fit_enc.bin'. The size in line 455: 4020 bytes are however correct.

0 Kudos

429 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport
0 Kudos