I.MX8MMini : fsl-image-validation-imx-imx8mmevk.sdcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8MMini : fsl-image-validation-imx-imx8mmevk.sdcard

866 Views
santhosh2
Contributor IV

Hi,

Every change in the linux kernel and compiling using bitbake "virtual/kernel" -c compile -f and then doing a  bitbake fsl-image-validation-imx is taking lot of time near 3 hrs for single compilation. Is there any other way ...? so that we can modify the kernel and update in fsl-image-validation-imx-imx8mmevk.sdcard  rootfs

Also let us know, How do i mount the fsl-image-validation-imx-imx8mmevk.sdcard and update the linux image and then again convert it to fsl-image-validation-imx-imx8mmevk.sdcard

Regards

Santhosh

0 Kudos
Reply
1 Reply

751 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Santhosh,

For modifying u-boot code and kernel / device, you have 2 ways to save building time.

1. Using Yocto

(1) u-boot

--> bitbake u-boot-imx -f -c compile

--> bitbake u-boot-imx -c deploy

(2) kernel

--> bitbake linux-imx -f -c compile

--> bitbake linux-imx -c deploy

2. Using standalone for u-boot / kernel

see the link, please!

Detailed Operations For Standalone On Linux BSP of I.MX Processors 

or see following linux documents:

--i.MX_Linux_User's_Guide.pdf

--i.MX_Porting_Guide.pdf

open document, and search "standalone", you will see steps on how to ...

...

How to build U-Boot and Kernel in standalone environment

...

[Comment]

If you don't have documents of linux BSP, download it here, please!

Embedded Linux for i.MX Applications Processors | NXP 

Hope above information is helpful for you!

Have a nice day!

B.R,

Weidong

0 Kudos
Reply