I.MX8M would automatically crashes under do not do anything

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8M would automatically crashes under do not do anything

6,862 Views
dylan_lin
Contributor III

Hello experts ,

I found my I.MX8M board would automatically crashes under do not do anything,

( can't output log or key any command )

it might happen between 1~2 hour,

but after  i keyin suspend order , the I.MX8M would not crash ,

this scenario can't happen in heavy loading and any also can't happen in any thread was running.

Device information as below:

CPU : MIMX8MQ6CVAHZAB

LPDDR4 : MT53B768M32D4NQ-062 WT:B

PMIC : PF4210

Labels (1)
24 Replies

5,121 Views
hthiery
Contributor I

Hi Igor,

is it possible to get this mentioned document. We see the same issue on our board.

BR,

Heiko

0 Kudos

3,216 Views
dylan_lin
Contributor III

Dear  Igor

It is not I.MX8M evk , but i used LPDDR4 512MB and 4GB to design in this case,

as so far , we tried to build 512MB and 4GB two versions base on the Linux 4.14.98.2.20,

the 4GB and 512MB both of two version crashed under do nothing , but 512MB version always crashed

between 1~2 hours , the 4GB version can stay idle 2~3 days.

this issue was so hardly to find out the root cause , because it was not to log out , and cant key in

any commands .

Do you have any thoughts and directions on this issue?

0 Kudos

924 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dylan

 

could you try to reproduce issue on i.MX8M EVK with latest

Demo Image  Linux Binary Demo Files - i.MX 8MQuad EVK

If issue can not be reproduced, suggest to rerun ddr test and update image

with new lpddr4 calibration settings.

https://community.nxp.com/docs/DOC-340179 

 

Best regards
igor

0 Kudos

881 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dylan

if this is i.MX8M EVK, may be recommended to try latest

Demo Image  Linux Binary Demo Files - i.MX 8MQuad EVK

from software link i.MX Software | NXP 

If this will not help nxp has return service: Returns and Warranty Information | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos