When using NXP I.MX8M Plus chip for bare metal development and debugging, and using DStream emulator to connect to the JTAG interface of I.MX8M Plus processor through JTAG, pin JTAG_ MOD has been set to low level, but the development board cannot enter the JATG debugging mode, and the ROM Table of the chip cannot be read using the J-Link emulator. Does the I.MX8M Plus chip disable the JTAG function when it leaves the factory? How can I enable the Cortex-A53 processor in I.MX8M Plus chip to enter the bare metal debugging mode through JTAG? Thank you
Hello,
Yes, JTAG is disable when is leaving the factory, but this is just for rom access you can access to the rest of the code.
Regards
if i no use rom access, how can i do that use the jtag for debug Cortex-a53 bare metal program ?
how can i do that enter jtag debug mode, thank you