I.MX8 Mini gpio pins output type?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8 Mini gpio pins output type?

1,001 Views
faiz
Contributor I

Hello,

1) When the GPIO pins are configured as output pins, what is the output type? Can we choose between push pull and open drain? I couldn't find this information in the datasheet.

2) I have to use a level shifter for the GPIO pins. Would you see an issue with using: http://www.ti.com/product/TXS0108E?dcmp=dsproject&hqs=pf?

Thank you,

Faiz

0 Kudos
Reply
1 Reply

905 Views
Yuri
NXP Employee
NXP Employee

Hello,

1.

  IMX8Mm output pins can be configured as CMOS or as open drain, using corresponding

Pad Control Register.  

2.

  Customers can use the mentioned shifter.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply