I.MX7 power sequencing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX7 power sequencing

1,920 Views
NIKHITHAANTONY
Contributor I

In the datasheet of I.MX7 it is given that, VDD_SOC should powerup before NVCC_DRAM and NVCC_DRAM_CKE. So whether it can be done by software. In hardware design, whether we need to take care anything for delaying NVCC_DRAM and NVCC_DRAM_CKE

0 Kudos
Reply
5 Replies

1,902 Views
NIKHITHAANTONY
Contributor I

Then How VDD_SOC will become high before NVCC_DRAM and NVCC_DRAM_CKE.

0 Kudos
Reply

1,896 Views
igorpadykov
NXP Employee
NXP Employee

>How VDD_SOC will become high before NVCC_DRAM and NVCC_DRAM_CKE

 

in hardware. Use appropriate PMIC with power-up sequence compatible with i.MX7D datasheet

requirements.

 

Best regards
igor

0 Kudos
Reply

1,888 Views
NIKHITHAANTONY
Contributor I

We designed I.MX7 processor as per SABRE board. In that PMIC PF3000 is used. 

So there will be correct power sequencing..right?

0 Kudos
Reply

1,883 Views
igorpadykov
NXP Employee
NXP Employee

>We designed I.MX7 processor as per SABRE board. In that PMIC PF3000 is used. 

>So there will be correct power sequencing..right?

 

right

0 Kudos
Reply

1,908 Views
igorpadykov
NXP Employee
NXP Employee

Hi NIKHITHA

 

>whether it can be done by software..

 

no

 

>whether we need to take care anything for delaying NVCC_DRAM and NVCC_DRAM_CKE

 

no need.

 

Best regards
igor

0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----