I.MX6ULL minicom USB connecting problem(ttyUSB0)

cancel
Showing results for 
Search instead for 
Did you mean: 

I.MX6ULL minicom USB connecting problem(ttyUSB0)

419 Views
kzy545
Contributor I

Hellow

I'm trying to use I.MX6ULL but i have a problem of minicom

222.png

It is i connected board with SD card which has booting image

And than i run minicom and do setting like that

3333.png

after setting i did run minicom again to connect with my board but when i run minicom i could not connect with my board like that

4444.png111.PNG

Also, i could not find 'ttyUSB0' in the /dev

Now, i am expecting SD card doesn't have exact booting image or use another USB Port

Could you hele me sort my problem out?

Labels (2)
0 Kudos
1 Reply

290 Views
radhikasomaiya
Senior Contributor II

Hi Shinbok KIM,

Hope you have connected USB Debug cable to J1901 on the base board (mentioned in Quick start Guide for imx6ULL).