I.MX6ULL Whether to support 8 megapixel camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6ULL Whether to support 8 megapixel camera

577 Views
刘卫强刘
Contributor I

I want to develop a handheld product using i.mx6ull. The camera needs 8 million pixels. I don't know if the CSI interface of i.mx6ull can support it.

0 Kudos
3 Replies

500 Views
art
NXP Employee
NXP Employee

No, the CSI interface of the i.MX6ULL processor cannot support a 8Mpixel camera. The maximum theoretical camera resolution supported is 4Mpixel.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

500 Views
刘卫强刘
Contributor I

Hi,Artur:

       In the 6UL training slides PPT I see the following description:

Data bus
- Up to 24-bit
- Also support 8-bit, 10-bit and 16-bit
Variety of data formats
- YUV 4:2:2/4:4:4,
- RGB 16/24 bpp
- CCIR656
- Other: as generic data, including compressed streams
Frame resolution:
- Essentially unlimited (up to 65535 x 65535 pixels)
Input rate:
- 200 MPixel/s peak

Is the 6ull and 6ul CSI interfaces consistent? Can the 6ull input rate reach 200MPixel/s, and if so, can 8MPixel @25fps be possible?

0 Kudos

500 Views
刘卫强刘
Contributor I

     Hi,Artur:

           How is this pixel converted, is there any basis for reference in the manual? Thank you!

0 Kudos