I.MX6ULL Evk booting emmc/SD using USB through DFU mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX6ULL Evk booting emmc/SD using USB through DFU mode

5,054 次查看
nagaprasad
Contributor I

Hi all,

Could anyone suggest how to boot os using USB in dfu mode? i tried to enable dfu command in u-boot but getting error as shown in the attachment.

Thanks&Regards,

NagaPrasad.

 

0 项奖励
回复
3 回复数

5,023 次查看
nagaprasadvasam
Contributor III

Dear Yuri,

we are developing an custom board based on IMX6ULL Evk, we need to flash os to emmc without having sd card, is it possible to flash emmc without need of having sd card, please suggest us to flash emmc through usb or any other process.

Thanks & Regards,

NagaPrasad.

0 项奖励
回复

5,018 次查看
Yuri
NXP Employee
NXP Employee

@nagaprasadvasam 
Hello,

   customers can use the UUU. Please refer to section 4.2 (Universal update utility)
of i.MX Linux® User's Guide.

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

Regards,
Yuri.

0 项奖励
回复

5,047 次查看
Yuri
NXP Employee
NXP Employee

@nagaprasad 
Hello,

     The following Community discussion shows how USB boot can be implemented.

https://community.nxp.com/t5/i-MX-Processors/iMX6ull-boot-from-USB-stick-with-uuu-mfgtools-Kernel-pa...

 

Regards,
Yuri.

0 项奖励
回复