I.MX6ULL Evk booting emmc/SD using USB through DFU mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6ULL Evk booting emmc/SD using USB through DFU mode

1,713 Views
nagaprasad
Contributor I

Hi all,

Could anyone suggest how to boot os using USB in dfu mode? i tried to enable dfu command in u-boot but getting error as shown in the attachment.

Thanks&Regards,

NagaPrasad.

 

0 Kudos
Reply
3 Replies

1,682 Views
nagaprasadvasam
Contributor III

Dear Yuri,

we are developing an custom board based on IMX6ULL Evk, we need to flash os to emmc without having sd card, is it possible to flash emmc without need of having sd card, please suggest us to flash emmc through usb or any other process.

Thanks & Regards,

NagaPrasad.

0 Kudos
Reply

1,677 Views
Yuri
NXP Employee
NXP Employee

@nagaprasadvasam 
Hello,

   customers can use the UUU. Please refer to section 4.2 (Universal update utility)
of i.MX Linux® User's Guide.

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

Regards,
Yuri.

0 Kudos
Reply

1,706 Views
Yuri
NXP Employee
NXP Employee

@nagaprasad 
Hello,

     The following Community discussion shows how USB boot can be implemented.

https://community.nxp.com/t5/i-MX-Processors/iMX6ull-boot-from-USB-stick-with-uuu-mfgtools-Kernel-pa...

 

Regards,
Yuri.

0 Kudos
Reply