Hi ,
In dts/imx6ul-pinfunc.h , the MDIO/MDC PAD is defined as following:
#define MX6UL_PAD_GPIO1_IO06__ENET1_MDIO 0x0074 0x0300 0x0578 0x0 0x0
#define MX6UL_PAD_GPIO1_IO06__ENET2_MDIO 0x0074 0x0300 0x0580 0x1 0x0
but in IMX6ULLRM.pdf ,
ENET1_MDIO can only be mapped to 3 pads ,ENET1_MDIO ,ENET2_CRS , GPIO1_IO05
Which one is correct ?
Best Regards
Hi Jerry,
The Table 23-1. ENET1 External Signals and Table 23-2. ENET2 External Signals of RM are incorrect.
I will ask doc team to correct it.
Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------