There are 4 available parts according to IMX6ULCEC.pdf.
MCIMX6G2DVM05AA
MCIMX6G3DVM05AA
MCIMX6G2DVK05AA
MCIMX6G3DVK05AA
But FSL web site has one more part, MCIMX6G0DVM05AA.
It has 1 USB, 2 SPI, no FlexCAN, 1 I2S, 4 UART, 2 I2C, 4 PWM and 1 10/100 ETH.
i.MX 6UltraLite Applications Processor|Freescale
Are there more differences between MCIMX6G0DVM05AA and other parts?
Why does the datasheet have no information about MCIMX6G0DVM05AA?
解決済! 解決策の投稿を見る。
Hello,
The Datasheets in Table 1 (Ordering Information) shows just examples.
This is not full set of possible devices. Please use the FactSheet below for
more details about differences between i.MX6UL releases (“i.MX 6UltraLite Device Options”).
http://cache.freescale.com/files/32bit/doc/fact_sheet/IMX6ULTRALITEFS.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
The Datasheets in Table 1 (Ordering Information) shows just examples.
This is not full set of possible devices. Please use the FactSheet below for
more details about differences between i.MX6UL releases (“i.MX 6UltraLite Device Options”).
http://cache.freescale.com/files/32bit/doc/fact_sheet/IMX6ULTRALITEFS.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------