I.MX6UL ethernet problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6UL ethernet problem

1,500 Views
haifengjin
Contributor II

在使用I.MX6UL的时候用两路以太网,PHY是LAN8720,ID分别是0和1,我改完,冷启动,会出现:

root@freescale ~$ ifconfig eth1 up
ifconfig: SIOCSIFFLAGS: No such device

但是如果我reboot一下,两路网络都可以,多次重复试验,现象一样,但是同样的配置在demo板上没有出现,这种是什么现象

Labels (1)
0 Kudos
Reply
2 Replies

1,099 Views
cyndent
Contributor I

你好 这个问题您这有解决么?我现在也遇到同样的问题,但是不知道怎么解决

0 Kudos
Reply

1,099 Views
b36401
NXP Employee
NXP Employee

Possibly eth1 interface does not start up at power-on but with re-initializing it comes up fine.
Please make sure that the board meets the power-on sequence.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply