I am working on i.MX6UL and get the following event:
=> hab_status
Secure boot disabled
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x22 0x33 0x00
0x00 0x00 0x00 0x0f 0x00 0x90 0x80 0x00
0x00 0x01 0x20 0x00
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_TARGET (0x33)
ENG = HAB_ENG_ANY (0x00)
How to decode the event data to analyze the issue? Thanks in advance.
My csf file:
[Header]
Version = 4.2
Hash Algorithm = sha256
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS
Engine = CAAM
[Install SRK]
File = "/opt/cst-3.3.1/crts/SRK_1_2_3_4_table.bin"
Source index = 0
[Install CSFK]
File = "/opt/cst-3.3.1/crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem"
[Authenticate CSF]
[Install Key]
Verification index = 0
Target Index = 2
File= "/opt/cst-3.3.1/crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem"
[Authenticate Data]
Verification index = 2
Blocks = 0x00908400 0x00000000 0x0000bc00 "SPL"
解決済! 解決策の投稿を見る。
Hi @benguan
Based on the CTX = HAB_CTX_TARGET (0x33), It seems the given target region goes beyond the allowed regions.
You can try to check the hab block address when you build the bootloader or try to dump the built bootloader ivt structure, then to verify the load address, offset and length for blocks of the authentication data.
For decoding the date, please refer to HAB4_API.pdf that will be under the directory of doc with the downloaded cst tool.
Best regards
Harvey
Hi @benguan
Based on the CTX = HAB_CTX_TARGET (0x33), It seems the given target region goes beyond the allowed regions.
You can try to check the hab block address when you build the bootloader or try to dump the built bootloader ivt structure, then to verify the load address, offset and length for blocks of the authentication data.
For decoding the date, please refer to HAB4_API.pdf that will be under the directory of doc with the downloaded cst tool.
Best regards
Harvey