I.MX6Solox PCIE addin card?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Solox PCIE addin card?

Jump to solution
471 Views
stuff
Contributor II


Is there a way to use the i.mx6 solox mpu as part of an add-in pcie card?

Labels (1)
0 Kudos
1 Solution
375 Views
igorpadykov
NXP Employee
NXP Employee

Hi GM

please look at below link describing usage i.MX6 PCIe as endpoint,

this functionality can be used in add-on card

i.MX6Q PCIe EP/RC Validation System

Best regards

igor
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
376 Views
igorpadykov
NXP Employee
NXP Employee

Hi GM

please look at below link describing usage i.MX6 PCIe as endpoint,

this functionality can be used in add-on card

i.MX6Q PCIe EP/RC Validation System

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos