Hi all,
I'm working on a mx6SX SABRE-SBD board and I use the parallel display interface for the display. This works well on linux.
I try to add a splash screen in u-boot. I added follow defines in my configuration file.
#define CONFIG_VIDEO
#define CONFIG_VIDEO_IPUV3
#define CONFIG_SPLASH_SCREEN
#define CONFIG_SPLASH_SCREEN_ALIGN
#define CONFIG_BMP_16BPP
#define CONFIG_VIDEO_LOGO
#define CONFIG_VIDEO_BMP_LOGO
But I got some errors. How can simple add a splash screen logo?
Thanks for your help
Peter
Hi all
The spalsh screen will be clean directly when u-boot jump to kernel (memory map printed). Is there a configuration that cleans the whole memory?
What could be the problem? I use kernel 3.14.54 (linux-fslc-mx6).
Peter
Hello
Now it works witth the u-boot version 2015.10. I can load a bmp.
But kernel clean the screen while boot. How can I disable reinitialisation the framebuffer?
Peter