I.MX6SX M4 on U-Boot-FSLC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6SX M4 on U-Boot-FSLC

2,423 Views
nathanb_
Contributor III

Hello All,

I'm currently trying to set up a MX6SXSABRESD evaluation board using the latest yocto fsl-community-bsp of 1.8 (Fido).  This builds the distro with a 3.14 linux-imx kernel and a 2015 u-boot-fslc bootloader.

The kernel boots on the A9 fine, and I can access Linux with no problem.  However, I'm unable to get the M4 running.  I had the M4 running fine under the distribution that is provided by Freescale with the evaluation board (L3.10.53_1.1.0_ga_images).

My procedure (under u-boot) is such:

1) Load the M4 binary into QSPI

fatload mmc 2:1 0x80800000 m4_qspi.bin

sf probe 1:0

sf erase 0x0 9000

sf write 0x80800000 0x0 9000

2) Start the M4

sf probe 1:0

cp 0x78000000 0x007F8000 8

mw.l 0x020D8000 0xA0480529

The binary that I'm flashing with is a simple "Hello World" program.  I'm seeing no output on the M4 terminal when starting the M4.  I can also do an sf read and see that the program is properly written.  So the flashing of the QSPI is working fine as far as I can tell.

However, if I do a memory dump with the md command at address 0x78000000 after sf probe 1:0, I do not see the program in my current distribution.  In the original distribution I would.  What's going on here?  Any ideas?

Thanks.

Labels (3)
3 Replies

1,509 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

seems u-boot-fslc (community uboot) has not sufficient SX support so far,

as mentioned in

https://github.com/Freescale/meta-fsl-arm/commit/ca332324a9bde3e9cbc5e37e18677110cfc38f22

you can post this on for obtaining details

https://lists.yoctoproject.org/listinfo/meta-freescale

differencies between u-boot-fslc and u-boot-imx :

https://community.freescale.com/message/402940#402940

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,509 Views
nathanb_
Contributor III

I also tried a program which triggers a reset on the A9 from the M4.  As soon as I run it on an image from L3.10.53_1.1.0_ga_images, the A9 resets.  When I run it on the Yocto u-boot-fslc, it does nothing.  So it does not appear to be a UART configuration issue.

0 Kudos
Reply

1,509 Views
nathanb_
Contributor III

Yet another note:

Changing from u-boot-fslc to u-boot-imx seems to resolve the issues (as expected).

PREFERRED_PROVIDER_u-boot = "u-boot-imx"

PREFERRED_PROVIDER_virtual/bootloader = "u-boot-imx"