I.MX6Q parallel camera input freeze (Oreo 8)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Q parallel camera input freeze (Oreo 8)

571件の閲覧回数
l_bruni
Contributor II

Hi,

we're working on a board built around a Variscite Dart-Mx6q.

The board has an Analog Device ADV7181C to perform cvbs acquisition.

All works fine but if the analog input is switched to an empty one (no camera connected) the bt.656 video data stream  to imx6 parallel port stops and the camera application freeze.

The only way to get all working again is reboot the board.

Is there any workaround?

Thank you, kind regards.

Luca

ラベル(1)
1 返信

515件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Luca

unfortunately I am not aware workaround for such case, probably one can add

some code to application which would exit when there are no several incoming camera frames.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------