I.MX6Q parallel camera input freeze (Oreo 8)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q parallel camera input freeze (Oreo 8)

1,057 Views
l_bruni
Contributor II

Hi,

we're working on a board built around a Variscite Dart-Mx6q.

The board has an Analog Device ADV7181C to perform cvbs acquisition.

All works fine but if the analog input is switched to an empty one (no camera connected) the bt.656 video data stream  to imx6 parallel port stops and the camera application freeze.

The only way to get all working again is reboot the board.

Is there any workaround?

Thank you, kind regards.

Luca

Labels (1)
1 Reply

1,001 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luca

unfortunately I am not aware workaround for such case, probably one can add

some code to application which would exit when there are no several incoming camera frames.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------