I.MX6Q VPU encode framerate can't change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q VPU encode framerate can't change

743 Views
richarddestiny
Contributor III

Hi,all

           I‘m working  in IMX6Q   sabreasd  ,kernel:3.10.17 , mxc_vpu_test.out

         the question is:    when change the framerate of  the  encode in  VPU  for  H.264, and  use  stormpastedImage_3.png  to play the  stream,  and the  log of framerate is corrcected , but the  storm show the  framerate is  30,  i can't change it?

      why?

thanks for you reply

have a great day!

Ricard

Labels (1)
0 Kudos
4 Replies

556 Views
joanxie
NXP TechSupport
NXP TechSupport

what framerate do you change? did you double check if your camera can support the new framerate or not? maybe some camera only can support 30,15fps.

0 Kudos

556 Views
richarddestiny
Contributor III

Hi,Xie

        thanks for your replay,

        my camera is support 30、15fps,and when i  encode h.264 in 15fps, storm still show  me 30fps

       by the way,I'm used  yuv file  to encode

0 Kudos

556 Views
BiyongSUN
NXP Employee
NXP Employee

mxc_vpu_test.out is for video only. no av sync.  just for play using 30fps fixed rate.

mxc_vpu_test.out is not a player.

0 Kudos

556 Views
richarddestiny
Contributor III

Hi,Biyong

     thanks for your reply,

     I just use mxc_vpu_test.out  for encode, and use   storm which is an app of  windows to play video

have a great day

Ricahrd

0 Kudos