I.MX6Q SABRE SDP DDR3 routing rules violation.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q SABRE SDP DDR3 routing rules violation.

907 Views
technect
Contributor II

I am trying to reuse the DDR3 routing of SABRE SDP (LAY-27392_C.brd). While reviewing the routing of DDR3, I found the violation of the recommended routing rule in Hardware Development Guide document (IMX6DQ6SDLHDG).

For example, IMX6DQ6SDLHDG recommended that the address and control signal to match within +/- 25mils, but as a result of measuring the length between i.mx6 and DDR, there is maximum difference of 170 mils as below.

  

Signal NameU1-U2U1-U3U1-U4U1-U5
DRAM_A7 (mils)1842.0961840.8921840.5691840.7
DRAM_A10 (mils)1672.4261674.3511668.9431670.868
Tolerance between signals (mils)169.67166.541171.626169.832

When I reuse the DDR routing of LAY-27392_C.brd intactly, I am very apprehensive about the violation of the routing rule as above.

Is the skew possible to optimize using DDR3 calibration tool?

Can you give any advise?

Labels (2)
0 Kudos
Reply
1 Reply

739 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following iMX6 DDR3 Routing on Sabre Dual Lite board

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply