I.MX6Q SABRE AUTOMATIVE GPS PPS CONNECTION

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q SABRE AUTOMATIVE GPS PPS CONNECTION

1,002 Views
neavyseal
Contributor I

Dear All,

I have I.MX6Q Sabre Automative Infoteinment card. It has UART, power and some other signals on CN1 connector on its base board. I want to connect a GPS device which has PPS signal to it. Where should I connect PPS signal?

RS232 DCD and DTR signals do not exist on this connector.

There is only "GPS_INTERR_B" signal which might be suitable. What is this signal's function?

Thank you,

0 Kudos
Reply
2 Replies

706 Views
neavyseal
Contributor I

Dear Victor,

Thank you so much,

Since I do not know very much about Linux kernel, I need additional information. How can I use this code? Should it be patched to the kernel?

0 Kudos
Reply

706 Views
b36401
NXP Employee
NXP Employee

You can refer this common recommendations regarding to driving PPS with GPIO pin:

http://lxr.free-electrons.com/source/Documentation/devicetree/bindings/pps/pps-gpio.txt
http://www.linuxpps.org/pipermail/discussions/2013-April/004423.html

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply