I.MX6Q OpenGL 2 application and awful performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Q OpenGL 2 application and awful performance

1,631件の閲覧回数
mimeline
Contributor I

I have a Java OpenGL 2 application. It can be launched but it is so slow. I guess it is because of the software mode.

How can I do to have hardware mode ? I have some errors in Xorg.0.log about drm :

 

[ 25.592] drmOpenDevice: node name is /dev/dri/card0

 

[ 25.604] [drm] failed to load kernel module "vivante"

 

[ 25.604] (EE) [drm] drmOpen failed.

 

[ 25.604] (EE) VIVANTE(0): [dri] DRIScreenInit failed. Disabling DRI.

 

[ 25.604] (==) RandR enabled

 

The whole log file is joined to this post.

Is there anything which can be done to enable hardware mode ?

 

Regards

Original Attachment has been moved to: Xorg.0.log.zip

ラベル(2)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,256件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Are you using Ubuntu?

Is your app using OpenGL ES 2.0 or desktop OpenGL?

Michel

0 件の賞賛
返信

1,256件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

No update from customer

0 件の賞賛
返信