My new project used MCU is I.MX6DL , it has tow USB ports ,one port use as a host ,and one port use as a device . now my question is why the USB device port alway has 4.4V output from USB_OTG_VBUS?
Hello Igorpadykov:
The first ,thanks your good support ,but I still can't understand why the 3P0 VBUS_sel registor set to 1 and the USB_OTG_VBUS output 4.4V from MCU itself. but if VBUS_sel set to 0 ,the USB_OTG_VBUS is 0.38V ,could you please help explain what is difference between VBUS_sel registor set to 0 and 1?
Hi zhongwei
in i.MX6DL this is input, so probably it is connected somewhere
on board to 4.4V, other reason is that chip may be damaged.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igorpadykov:
After we analysised ,we fond that if 3p0 registor bit7(VBUS_SEL) was set 0, measured the voltage of USB_OTG_VBUS is about 0.38V. i don't know why? could you please help explain it .thanks so much.
please look at Figure 50-1. Power system overview
i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf
Best regards
igor