I.MX6 lvds LC420EUN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 lvds LC420EUN

Jump to solution
2,211 Views
philipfeng
Contributor I

Hi everybody,

  I got a problem with I.MX6 connect to LG's LCD screen LC420EUN by LVDS .

  This is a LCD with resolution 1920x1080 .

  I changed the uboot param to LDB-1080P60 mode , and the lcd not work correctly.

  After read some document , I know I should change the configure of the fb_videomode struct in ldb.c .

  But the LCD TIMING TABLE describe as below , and I don't know how to config the fb_videomode param , did any body know ?

QQ图片20151214115356.png

Tags (2)
0 Kudos
Reply
1 Solution
1,655 Views
jayaramks
Contributor III
0 Kudos
Reply
2 Replies
1,656 Views
jayaramks
Contributor III
0 Kudos
Reply
1,655 Views
igorpadykov
NXP Employee
NXP Employee

Hi Philip

For 3.10.31 kernel, the attached patch was needed, the video mode is as followed.

For 3.10.17 kernel and older versions, just add the followed video mode:

video=mxcfb0:dev=ldb,LDB-1080P60,if=RGB24,bpp=32 ldb=spl1

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply