I.MX6 SATA problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 SATA problem

2,081 Views
sunfrank
Contributor I

Hi, community

       I meet a problem of SATA 

       hardware :  Imx6q core board + carrier   

       OS :  LINUX 3.0.35  

       SATA device :  I tried  both  HDD and SSD

       when power on we can see this information from serial port: 

....

Uniform Multi-Platform E-IDE driver
ide-gd driver 1.18
ahci: SSS flag set, parallel bus scan disabled
ahci ahci.0: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
ahci ahci.0: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
scsi0 : ahci_platform
ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02200fff] port 0x100 irq 71
GPMI NAND driver registered. (IMX)

.....

and later:

ata1: SATA link down (SStatus 0 SControl 300)

I use external power for HDD, so power is stable. 

0 Kudos
Reply
2 Replies

1,640 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sun

in general for better signal shape one can try to tweak IOMUX GPR13 register.
IOMUX GPR13 defines various SATA Phy transmitter/receiver settings.

Is it working in uboot, if yes then one can try to change configurations for IOMUXC_GPR13 to be same
in kernel as in U-boot (helped some customers).

diff --git a/arch/arm/mach-mx6/board-mx6q_sabresd.c b/arch/arm/mach-mx6/board-m

index ac9b8f8..95e5f2a 100644
--- a/arch/arm/mach-mx6/board-mx6q_sabresd.c
+++ b/arch/arm/mach-mx6/board-mx6q_sabresd.c
@@ -1177,7 +1177,7 @@ static int mx6q_sabresd_sata_init(struct device *dev, voi
         *.tx_edgerate_0(iomuxc_gpr13[0]),
         */
        tmpdata = readl(IOMUXC_GPR13);
-       writel(((tmpdata & ~0x07FFFFFD) | 0x0593A044), IOMUXC_GPR13);
+       writel(((tmpdata & ~0x07FFFFFD) | 0x0593E4C4), IOMUXC_GPR13);

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,640 Views
sunfrank
Contributor I

Hi,

         thank you very much for your reply.  my kernal can detect the HDD now,renson is the .config, lack of SATA support.   but the new problem is in android 4.4 , still can not detect the HDD, I found a document which says can modify the vold.fstab in ../system/etc,to set the HDD as a SD card.  but it seems like vold.fstab is not exsist any more after android 4.4...do you know another way to let android support the sata disk? 

0 Kudos
Reply