I.MX6 MMDC 32Khz refresh clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 MMDC 32Khz refresh clock

1,052 Views
rostyslavkhudol
Contributor III

Hi all,

I'm struggling to find which 32KHz clock is used by MMDC to perform a periodic auto refresh (ch.

46.4.8)? Is it coming from XTALOSC? It seems to be quite unstable.

Labels (1)
2 Replies

848 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rostyslav

you are right, for that reason recommended to use precision 32.768 kHz

oscillator as stated in Table 2-7. Oscillator and clock recommendations

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

848 Views
attilasukosd
Contributor I

As a feedback to NXP, I feel like this could be highlighted a lot more in the design guidelines, hardware design checklist, etc.

We've spent a lot of time debugging undefined behaviour with RAM, watchdog, USB, CEC etc on our custom designed board, only to realize that all of it was due to the inaccuracy of the internal 32kHz clock, which at certain temperatures fluctuated between 14-100kHz.

I'd go as far as to put it in the hardware design checklist explicitly that an external 32kHz clock is a requirement for proper function.