I.MX6 MIPI DSI problem with platform SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 MIPI DSI problem with platform SDK

2,826件の閲覧回数
hakanakis
Contributor I

Hello,

I am using  i.mx6dl sabre sd board and MIPI DSI display connected by MIPI expansion port. Display panel has HX8363A controller on it.

I have configured linux dts files and bootcmd, wrote new display panel driver for HX8363A display panel. It is working as intented. However, I cannot be able to display image with baremetal sofware.

I have to achieve this with baremeral software. With platform SDK software, I am conducting ipu tests. LDB tests are succesful. There is also MIPI DSI tests under Platform SDK. I am wondering whether MIPI DSI tests under Platform SDK is working or not? I have modified MIPI DSI tests for HX8363A display panel, but tests are failed. No image is displayed. I don't know what i am missing. What can be the problem? 

ラベル(6)
0 件の賞賛
返信
3 返答(返信)

2,462件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi hakan

one can try to run these tests on Sabre SD reference board using

sect.5. MIPI test SDK Unit Test Procedures.pdf included in SDK /doc

folder.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,462件の閲覧回数
hakanakis
Contributor I

I have tried to run these tests but they didnt work. I have changed the LCD_INIT fuction according to the display panel used(hx8363A) and also display panel channel structure to update timings. I guess that my problem is with CCM configuration. What are the necessary clock setting(values, clock route etc.) for proper operation of MIPI DSI and IPU?

0 件の賞賛
返信

2,462件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

SDK provided "as is", without support.

In general one can printf DSI registers in linux and compare with SDK.

Best regards
igor

0 件の賞賛
返信