I.MX6_MAX Latency with Miracast

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6_MAX Latency with Miracast

835 Views
rajvikamdar
Contributor III

Hi All

We have 2 nitrogen_6max devices, 1 as miracast source and 1 as miracast sink. Both the boards are running on Android 4.1.3. We are using oc5640 camera module.

On miracast capture and display we are getting video latency of about 400 ms.

When miracast starts at sink side we are getting below error. We are doubting if this is the issue:

E/BufferQueue(  110): [SurfaceView] query: BufferQueue has been abandoned!
E/ACodec  (  113): [OMX.Freescale.std.video_decoder.avc.v3.hw-based] NATIVE_WINDOW_MIN_UNDEQUEUED_BUFFERS query failed: No such device (19)
E/BufferQueue(  110): [SurfaceView] dequeueBuffer: BufferQueue has been abandoned!
E/ACodec  (  113): dequeueBuffer failed.
W/BufferQueue(  110): [SurfaceView] cancelBuffer: BufferQueue has been abandoned!
W/BufferQueue(  110): [SurfaceView] cancelBuffer: BufferQueue has been abandoned!
W/BufferQueue(  110): [SurfaceView] cancelBuffer: BufferQueue has been abandoned!
W/BufferQueue(  110): [SurfaceView] cancelBuffer: BufferQueue has been abandoned!
W/BufferQueue(  110): [SurfaceView] cancelBuffer: BufferQueue has been abandoned!
I/vpu-lib (  113): <gpu> free handle: 0x77cb3878, paddr: 0x6868b000, vaddr: 0x6f390000
I/vpu-lib (  113): <gpu> free handle: 0x77cb3850, paddr: 0x6818b000, vaddr: 0x6ee90000
I/vpu-lib (  113): <gpu> free handle: 0x77cb4960, paddr: 0x68c84000, vaddr: 0x6f989000
I/TunnelRenderer(  651): notify 7, 0, 0
I/TunnelRenderer(  651): message not care about
W/NetworkSession(  651): Error writing to pipe (Bad file number)
We need to achieve atleast a latency of 100ms-200ms. Your help would be highly appreciated.
Our commercial production is at stake because of the same.
Kind Regards
Rajvi
0 Kudos
2 Replies

637 Views
sandipsathvara
Contributor I

Hi,

Any update here?

0 Kudos

637 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandip

please proceed with professional services support as suggested on

WFD Sink for Linux 

Best regards
igor

0 Kudos