I.MX6 IPU blanking display smear issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 IPU blanking display smear issue

716 Views
zc_tee
Contributor III

Dear all,

I am currently using a i.mx6 Dual board on my task.

However when i do blanking: echo 1 > /sys/class/graphic/fb0/blank

the lvds display becomes smear, instead of turn blank (full black).

Is there anyway i can make the screen blank (full black), instead of the smearing when do blanking?

Thank you.

Regards,

ZC

Tags (3)
0 Kudos
4 Replies

504 Views
joanxie
NXP TechSupport
NXP TechSupport

this command works for my board, did  you use dual display or just lvds?

if you use echo "0"  to fb0, any issue?

0 Kudos

504 Views
zc_tee
Contributor III

Hi Guanqiong Xie,

echo "0" will return the display to normal mode, is ok.

we are using dual display. both LVDS output at 800x600 resolution.

Regards,

Tee

0 Kudos

504 Views
joanxie
NXP TechSupport
NXP TechSupport

lvds is for fb0 or fb2? could you send the uboot command to me?

0 Kudos

504 Views
zc_tee
Contributor III

Hi Guanqiong Xie,

LVDS is for both fb0 and fb2.

We did not set it in uboot command. instead we hardcode it in the kernel source code.

Display is ok cause we always can see both display show correctly, besides this blanking issue.

Regards,

Tee

0 Kudos