I.MX6 DDR Calibration Fail with EMCP memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 DDR Calibration Fail with EMCP memory

2,192 Views
david5icp
Contributor III

Hi Community,

  We has a new design using IMX6q with emcp (LPDDR2 + eMMC, Micron MT29PZZZ8D5BKFTF) chip. I want to use ddr calibration tool to get paramater for ddr, I had try several different config files to test my board. But allways fail and show "ERROR FOUND, we can't get suitable value !!!!"

  Does it support this emcp memory ? And who i to check it ? Thanks!

Original Attachment has been moved to: MX6Solo_lpddr2-17.inc.zip

Original Attachment has been moved to: Calibration-Fail.log.zip

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,554 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try using the recent DDR stress test (it provides calibration options too).

i.MX6/7 DDR Stress Test Tool V2.52

  Also, it makes sense to check PCB trace requirements :

- DQS signals should be 5 – 200 mils shorter than the clocks.

- Data and respective DQM signals should be 5 – 25 mils shorter than

  corresponding DQSs.

- Address and control signals should be 5 – 25 mils shorter than the clocks.

- Longest clock trace must be <= 3 inches.

  As for DRAM configuration tool, please try the following

i.MX6DQ LPDDR2 Register Programming Aid

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------