Hi, I have a question for boot config pins for EMMC in i.MX6.
I want to confirm that BOOT_CFG4 is not used for EMMC, so I don't care those pins in boot time.
In reference schematics, those pins are all LOW status, but it has no problem to pull up them, is it right?
Thank you.
已解决! 转到解答。
Hi JHY
I think you are right, except BOOT_CFG4[7] - OEM Infinite Loop Enable
it should be low (i.MX6DQ Reference Manual Table 8-2. Boot eFUSE Descriptions).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi JHY
I think you are right, except BOOT_CFG4[7] - OEM Infinite Loop Enable
it should be low (i.MX6DQ Reference Manual Table 8-2. Boot eFUSE Descriptions).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------