I.MX6 BOOT CONFIG for EMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 BOOT CONFIG for EMMC

Jump to solution
2,026 Views
JHY
Contributor IV

Hi, I have a question for boot config pins  for EMMC in i.MX6.

I want to confirm that BOOT_CFG4 is not used for EMMC, so I don't care those pins in boot time.

In reference schematics, those pins are all LOW status, but it has no problem to pull up them, is it right?

Thank you.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,499 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

I think you are right, except BOOT_CFG4[7] - OEM Infinite Loop Enable

it should be low (i.MX6DQ Reference Manual Table 8-2. Boot eFUSE Descriptions).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
1,500 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

I think you are right, except BOOT_CFG4[7] - OEM Infinite Loop Enable

it should be low (i.MX6DQ Reference Manual Table 8-2. Boot eFUSE Descriptions).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,499 Views
JHY
Contributor IV

Thank you, Igor.

I have one more question.

How about BOOT_CFG3[0] [1] [3]?

It is reserved pin and reference EVK has always low status.

Is it must be low in boot time for eMMC?

0 Kudos
Reply
1,499 Views
igorpadykov
NXP Employee
NXP Employee

Hi JHY

for eMMC boot they can be left unconnected

Best regards

igor