Hi
I am using ubuntu 11.10 as host system and succesfully build a new images for ubuntu ( u-boot.bin, uImage, anf file system) for I.MX53 QSB, using the steps mentioned in CreateUbuntu1110ltib110901.docx, however i could not install git-core,and i could not find /etc/inetd.conf in my host system.
neither i could not start the board with these new images, nor anything is coming at minicom can any one tell me what could be the resaon for this.
However I just needed the new uImage so I used u-boot-mx53-loco.bin which is prebuilt image given by freescale, after this i could see booting happening but it fails to load file system, the log is like this
**********************************************************************************************************************************************
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p1): using internal journal
EXT3-fs (mmcblk0p1): recovery complete
EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:1.
Freeing init memory: 172K
starting pid 1210, tty '': '/etc/rc.d/rcS'
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
Setting the hostname to freescale
Mounting filesystems
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
cp: write error: No space left on device
mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
starting pid 2257, tty '': '/sbin/getty -L ttymxc0 115200 vt100
arm-none-linux-gnueabi-gcc (4.4.4_09.06.2010) 4.4.4
root filesystem built on Sat, 23 Mar 2013 18:32:24 +0530
Freescale Semiconductor, Inc.
freescale login:
**********************************************************************************************************************************************
Can any one tell me resons for these two problems
已解决! 转到解答。
Please apply the BSP 11.09 patch.
You can download the BSP and patch from the i.MX53QSB web page:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
BSP : L2.6.35_11_09_ER_SOURCE
Patch : IMX53_LINUX_1109_BSP_PATCH
Also, you can try the "MX53_QSB_UBUNTU_SD_DEMO_IMAGE". It contain the Ubuntu filesystem for i.MX53QSB.
I again tried to build images for IMX53 QSB with different kernel version 2.6.38 using LTIB, but with this, building failed
with this log
************************************************************************************************************************************************************
make[1]: *** [ScreenLayer.o] Error 1
make[1]: Leaving directory `/home/praveen/L2.6.35_11.09.01_ER_source_bundle/ltib/rpm/BUILD/imx-lib-11.09.01/screenlayer'
make: *** [screenlayer] Error 2
error: Bad exit status from /home/praveen/L2.6.35_11.09.01_ER_source_bundle/ltib/tmp/rpm-tmp.96851 (%build)
RPM build errors:
Bad exit status from /home/praveen/L2.6.35_11.09.01_ER_source_bundle/ltib/tmp/rpm-tmp.96851 (%build)
Build time for imx-lib: 6 seconds
Failed building imx-lib
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Mon Mar 25 15:49:58 2013
Ended: Mon Mar 25 16:13:00 2013
Elapsed: 1382 seconds
These packages failed to build:
imx-lib
Build Failed
Exiting on error or interrupt
************************************************************************************************************************************************************
I am attaching complete log
Please apply the BSP 11.09 patch.
You can download the BSP and patch from the i.MX53QSB web page:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
BSP : L2.6.35_11_09_ER_SOURCE
Patch : IMX53_LINUX_1109_BSP_PATCH
Also, you can try the "MX53_QSB_UBUNTU_SD_DEMO_IMAGE". It contain the Ubuntu filesystem for i.MX53QSB.