I.MX502 Max CS and the memory size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX502 Max CS and the memory size

ソリューションへジャンプ
2,236件の閲覧回数
norishinozaki
Contributor V

Hello,

I need use 5 CSs to configure CS0(64MB), CS1(32MB), CS2(32MB), CS3(32MB), CS4(32MB) in i.MX502 based system.

In the IMX50RM the page 150, it says,

Off Chip Memories

The supported configurations are

• CS0(128M), CS1 (0M), CS2 (0M),CS3(0M)

• CS0(64M), CS1(64M), CS2(0M), CS3(0M)

• CS0(64M), CS1(32M), CS2(32M),CS3(0M)

• CS0(32M), CS1(32M), CS2(32M),CS3(32M)

However in the latter page, in the "23.2 Featrus".

It says:

• Up to four chip selects for external devices

• Flexible address decoding. Each chip select memory space determined separately, according to VIA port configuration (see Chip Select Memory Map).

Configurable Chip Select 0 base address (by VIA)

• Individual select signal for each one of the memory space defined. Up to 6 memory spaces may be defined and programmed individually.

• 128-bit external address bus, max memory size can be 256MByte (2 Gigabit).

Seems like max 6 memory spaces with 256MB might be possible.

Is it really possible?

Best regards,

Nori Shinozaki

ラベル(1)
0 件の賞賛
返信
1 解決策
2,158件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,159件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,159件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

correct description is given in page 150 -

this is specific i.MX50 implementation of EIM module, while

sect 23.2 Features gives generic description of EIM

module.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,159件の閲覧回数
norishinozaki
Contributor V

Hollo Igor,

Thank you, I'm planing to increase a CS by adding external logic.

I couldn't find EIM's max fan-out number in the datasheet.

Can i.MX502 fanout total 5 CSs?

Best regards,

Nori Shinozaki

0 件の賞賛
返信
2,159件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nori

i.MX50 has CSn described on page 150, seems

one can add some logic for additional "fan-out number".

Best regards

igor

0 件の賞賛
返信
2,159件の閲覧回数
norishinozaki
Contributor V

Igor,

Thanks, I read this description.

But not sure about the max fan-outs from the DC characteristics stand point.

Best regards,

Nori Shinozaki

0 件の賞賛
返信