I.MX280 Touch screen controller.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX280 Touch screen controller.

1,278件の閲覧回数
russellholmes
Contributor I

Hello all,

Hoping to get a quick and concise answer on this one!

Does the MCIMX280DVM4B come with a touch screen controller interface? I know the MCIMX283DVM4B uses some pins on the LRADC as a touch screen controller.

I was hoping that this is the same for the MCIMX280DVM4B.


Thanks in advance!!

ラベル(2)
0 件の賞賛
返信
1 返信

1,178件の閲覧回数
Yuri
NXP Employee
NXP Employee

  According to Table 2 (i.MX28 Functional Differences) of the i.MX28

Datasheet  (IMX28CEC, Rev. 3, 07/2012) the i.MX280 supports the LRADC.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信