I.MX Yoco Liux meta-rust layer issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX Yoco Liux meta-rust layer issue

1,226 Views
_ZZ_
Contributor II

Hello everyone,

I am experiencing an I.MX yocto build error related to the meta-rust layer which I was not seeing before during the bitebake building process. below it the error line, 

ERROR: Task (virtual:native:/home/dand/yocto/sti_git_repos/firmware_yocto/poky/../meta-rust/recipes-devtools/rust/rust_1.43.0.bb:do_compile) failed with exit code '1'

I wonder if anyone has seen this before and knows the solution

thanks,

0 Kudos
Reply
2 Replies

1,169 Views
_ZZ_
Contributor II

after few times trying, it just went though successfully. not sure what was wrong. It is OK now

1,209 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello!

It make me thing that the Rust version that you are using is not compatible. Please check if the version that you are using is the correct.

 

Best regards!

0 Kudos
Reply
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----