I.MX 6DL OTA update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX 6DL OTA update

573 Views
varunjeevangoud
Contributor I

HI Guys, 

               VARUN here, having issues with OTA update for Android 6.0.1_r22 and kernel 4.1.15. 

I have been following the same procedure to  build recovery.img to perform OTA operation mentioned in the procedure Doc , but i'm not able to generate recovery.img. I tried some changes in Makefile in /build/core, still the result is fail!!. Any one can help me out..i have attached Make file from /build/core. Please have a look and come back.

 

This is results after the command make otapackage:

PRODUCT_COPY_FILES device/medallion/imx6/init.recovery.freescale.rc:root/init.recovery.freescale.rc ignored.
PRODUCT_COPY_FILES external/bluetooth/bluez/obexd/src/obexd:system/bin ignored.
PRODUCT_COPY_FILES device/medallion/imx6/etc/ueventd.freescale.rc:root/ueventd.freescale.rc ignored.
PRODUCT_COPY_FILES device/medallion/common/display/display_mode_fb0.conf:system/etc/display_mode_fb0.conf ignored.
PRODUCT_COPY_FILES device/medallion/common/display/display_mode_fb2.conf:system/etc/display_mode_fb2.conf ignored.
PRODUCT_COPY_FILES device/medallion/common/display/display_mode_fb4.conf:system/etc/display_mode_fb4.conf ignored.
make: *** No rule to make target `otapackage'. Stop.

 

This is results after the command make recoveryimage:

PRODUCT_COPY_FILES device/medallion/imx6/init.recovery.freescale.rc:root/init.recovery.freescale.rc ignored.
PRODUCT_COPY_FILES external/bluetooth/bluez/obexd/src/obexd:system/bin ignored.
PRODUCT_COPY_FILES device/medallion/imx6/etc/ueventd.freescale.rc:root/ueventd.freescale.rc ignored.
PRODUCT_COPY_FILES device/medallion/common/display/display_mode_fb0.conf:system/etc/display_mode_fb0.conf ignored.
PRODUCT_COPY_FILES device/medallion/common/display/display_mode_fb2.conf:system/etc/display_mode_fb2.conf ignored.
PRODUCT_COPY_FILES device/medallion/common/display/display_mode_fb4.conf:system/etc/display_mode_fb4.conf ignored.
make: Nothing to be done for `recoveryimage'.

0 Kudos
1 Reply

393 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Varun,

Are you still experiencing problems building the OTA package? Have you followed the instructions on the Android FAQ or Android User’s Guide without any changes (to prove functionality before customizing your image)?

Regards,

0 Kudos