I.MX 6( MCIMX6S5EVM10ADR) BPM Microsystem programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX 6( MCIMX6S5EVM10ADR) BPM Microsystem programming

1,158 Views
marco_villasana
Contributor I

Good afternoon, we are using the I.MX 6 in some of our products, we are currently using the NXP Mfg tool to program this device on board. We are willing to move this programing to a device level, prior to mounted on PCB, is it possible to program this micro using a programmer? (BPM machine in this case)

Labels (1)
0 Kudos
Reply
6 Replies

1,103 Views
igorpadykov
NXP Employee
NXP Employee

Hi Marco

i.MX6 have not internal program flash, they use external media like

sd, or nor which may be programmed using programmer.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,103 Views
marco_villasana
Contributor I

Thank you for your answer What about IMX8?

Regards!

0 Kudos
Reply

1,103 Views
igorpadykov
NXP Employee
NXP Employee

it is the same

Best regards
igor

0 Kudos
Reply

1,103 Views
marco_villasana
Contributor I

Thank you for the quick answer, so, just to be clear, the IMX6 and IMX8 can not be programmed using any kind of programmer right?

0 Kudos
Reply

1,103 Views
igorpadykov
NXP Employee
NXP Employee

right.

0 Kudos
Reply

1,103 Views
marco_villasana
Contributor I

Thanks for your attention

0 Kudos
Reply