I Closed boot my Board using HAB process; still my device shows as trusted mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I Closed boot my Board using HAB process; still my device shows as trusted mode?

跳至解决方案
1,433 次查看
swapnilpendhare
Contributor III

Hi,

I tried to close config my wandboard using Secure boot on Wandboard and I could see at uboot level I have close config

No panel detected: default to HDMI

     Display: HDMI (1024x768)

     In:    serial

    Out:   serial

    Err:   serial

    Net:   FEC [PRIME]   

    Hit any key to stop autoboot:  0

    => hab_status

    Secure boot enabled

    HAB Configuration: 0xcc, HAB State: 0x99

    No HAB Events Found!

I dont have my linux kernel enabled with close config certificates like u-boot.

Now when i try to check the snvs register i can see following

SSM_STsnvs-secvio 20cc000.caam-snvs: violation handlers armed - trusted state

How can set my board to secure state instead of trusted one.

Thanks and Regards,
Swapnil Pendhare.

标签 (2)
0 项奖励
回复
1 解答
1,213 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please check if SEC_CONFIG fuse is burned to close mode.

Mx6 HAB (High Assurance Boot)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,214 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please check if SEC_CONFIG fuse is burned to close mode.

Mx6 HAB (High Assurance Boot)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复