Hysteresis function on IOMUX receiver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hysteresis function on IOMUX receiver

Jump to solution
1,452 Views
t-iishii
Contributor II

Hello,

I try to understand about hysteresis function on IOMUX receiver by datasheet and

Influence of Pin Setting on System Function and Performance.

Following is a my understanding.

Is it correct?

      |   min  |   typ  |   max  |
------+--------+--------+--------+------
Vhys  |   250  |   ---  |   ---  | mV
 VT+  |0.5*ovdd|   ---  |   ---  | V
 VT-  |   ---  |   ---  |0.5*ovdd| V

0.5* 3.3  = 1.65
0.5* 1.8  = 0.9
0.5* 0.25 = 0.125

   transittion  |   ovdd  |  min
----------------+---------+-------
     L -> H     |   3.3   | 1.775 = 1.65+ 0.125
     L -> H     |   1.8   | 1.025 = 0.9 + 0.125

  transittion   |   ovdd  | max
----------------+---------+-------
     H -> L     |   3.3   | 1.525 = 1.65- 0.125
     H -> L     |   1.8   | 0.775 = 0.9 - 0.125


for ovdd=3.3v
             |
     +---------------+------
     |       |       |
     |       |       | T+ = 1.775
-----|-------+-------|----------
     |<------------->| Vhys = 250mV
     |       |       |
 ----+---------------+
     :       |
     :
     T- = 1.525


for ovdd=1.8v
             |
     +---------------+------
     |       |       |
     |       |       | T+ = 1.025
-----|-------+-------|----------
     |<------------->| Vhys = 250mV
     |       |       |
 ----+---------------+
     :       |
     :
     T- = 0.775

Best regards,

Ishii.

Labels (1)
0 Kudos
Reply
1 Solution
1,341 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,342 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,341 Views
t-iishii
Contributor II

Hello Yuri,

Thank you for your quick response.

I will answer it my customer.

Best regards,

Ishii.

0 Kudos
Reply