Hwclock: can't open '/dev/misc/rtc': No such file or directory imx6sl (custom imxl2evn10aa)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hwclock: can't open '/dev/misc/rtc': No such file or directory imx6sl (custom imxl2evn10aa)

ソリューションへジャンプ
19,820件の閲覧回数
RobertCorrellus
Contributor II

Custom build for imx6sl based on the imx6slevk, custom board built with a imx6L2evn10aa. Can't start RTC?  Hardware oscillator is running, verified with scope.

Uboot startup details:

U-Boot 2013.10 (May 07 2014 - 16:59:28)

CPU: Freescale i.MX6SL rev1.0 at 792 MHz

Reset cause: WDOG

Board: WEBBG3FLIGHT

DRAM: 1 GiB

MMC: FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In: serial

Out: serial

Err: serial

Net: FEC [PRIME]

Warning: failed to set MAC address

Hit any key to stop autoboot: 0

=> mtest 10095777 1095779

Testing 10095777 ... 01095779:

Pattern FFFFFFFF Writing... Reading...Iteration: 286

=>

U-Boot 2013.10 (May 07 2014 - 16:59:28)

CPU: Freescale i.MX6SL rev1.0 at 792 MHz

Reset cause: POR

Board: WEBBG3FLIGHT

DRAM: 1 GiB

MMC: FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In: serial

Out: serial

Err: serial

Net: FEC [PRIME]

Warning: failed to set MAC address

Hit any key to stop autoboot: 0

mmc0 is current device

mmc0 is current device

reading boot.scr

** Unable to read file boot.scr **

reading uImage

3798580 bytes read in 176 ms (20.6 MiB/s)

Booting from mmc ...

reading imx6sl-evk.dtb

** Unable to read file imx6sl-evk.dtb **

## Booting kernel from Legacy Image at 82000000 ...

  Image Name: Linux-3.0.35-4.1.0-webbg3flight+

  Image Type: ARM Linux Kernel Image (uncompressed)

  Data Size: 3798516 Bytes = 3.6 MiB

  Load Address: 80008000

  Entry Point: 80008000

  Verifying Checksum ... OK

  Loading Kernel Image ... OK

Starting kernel ...

Linux version 3.0.35-4.1.0-webbg3flight+g5fc7229 (rcorrellus@A665laptop) (gcc version 4.8.1 (GCC) ) #1 PREEMPT Wed May 7 17:07:31 EDT 2014

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Teledyne Webb Research Glider Processor

Memory policy: ECC disabled, Data cache writeback

CPU identified as i.MX6SoloLite, silicon rev 1.0

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260096

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk0p2 rootwait rw

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 1024MB = 1024MB total

Memory: 1027800k/1027800k available, 20776k reserved, 0K highmem

Virtual kernel memory layout:

  vector : 0xffff0000 - 0xffff1000 ( 4 kB)

  fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

  DMA : 0xf4600000 - 0xffe00000 ( 184 MB)

  vmalloc : 0xc0800000 - 0xf2000000 ( 792 MB)

  lowmem : 0x80000000 - 0xc0000000 (1024 MB)

  pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)

  modules : 0x7f000000 - 0x7fe00000 ( 14 MB)

  .init : 0x80008000 - 0x80038000 ( 192 kB)

  .text : 0x80038000 - 0x80aca4f4 (10826 kB)

  .data : 0x80acc000 - 0x80b2ca10 ( 387 kB)

  .bss : 0x80b2ca34 - 0x80b77b54 ( 301 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:624

MXC GPIO hardware

sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms

arm_max_freq=1GHz

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

devtmpfs: initialized

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 262144 B

bio: create slab <bio-0> at 0

print_constraints: vmmc: 3300 mV

SCSI subsystem initialized

spi_imx imx6q-ecspi.1: probed

spi_imx imx6q-ecspi.2: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

i2c i2c-2: Invalid 7-bit I2C address 0x00

i2c i2c-2: Can't create device at 0x00

mc_pfuze 2-0008: ID: 0,Full lay: 1 ,Metal lay: 1

mc_pfuze 2-0008: FAB: 0 ,FIN: 0

print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV

print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1300 mV

print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3150 mV

print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1200 mV

print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1200 mV

print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3300 mV

print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV

print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV

print_constraints: PFUZE100_VREFDDR: at 750 mV

print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1200 mV

print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 800 mV

print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 2500 mV

print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 1800 mV

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

cfg80211: Calling CRDA to update world regulatory domain

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 6, 262144 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

etb: probe of etb failed with error -2

etm: probe of etm.0 failed with error -2

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = c0820000 suspend_iram_base=c0818000

PM driver module loaded

IMX usb wakeup probe

cpu regulator mode:ldo_bypass

_regulator_get: get() with no identifier

mx6_cpu_regulator_init: failed to get pu regulator

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 2007

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

imx-uart.1: ttymxc1 at MMIO 0x2024000 (irq = 59) is a IMX

imx-uart.2: ttymxc2 at MMIO 0x2034000 (irq = 60) is a IMX

imx-uart.3: ttymxc3 at MMIO 0x2038000 (irq = 61) is a IMX

imx-uart.4: ttymxc4 at MMIO 0x2018000 (irq = 62) is a IMX

fsl_rngc fsl_rngc.0: FSL RNGC Registered.

loop: module loaded

m25p80 spi1.0: m25p32 (4096 Kbytes)

Creating 1 MTD partitions on "m25p32":

0x000000000000-0x000000400000 : "bootloader"

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

add wake up source irq 74

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.1: irq 74, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

mousedev: PS/2 mouse device common for all mice

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

i2c-core: driver [mma8450] using legacy suspend method

i2c-core: driver [mma8450] using legacy resume method

add mma8450 i2c driver

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

Bluetooth: Generic Bluetooth USB driver ver 0.6

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci sdhci-esdhc-imx.1: no write-protect pin available!

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA

Thermal calibration data is 0x59151169

Thermal sensor with ratio = 185

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

dcp dcp.0: DCP crypto enabled.!

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

usbcore: registered new interface driver snd-usb-audio

Cirrus Logic CS42888 ALSA SoC Codec Driver

i2c-core: driver [cs42888] using legacy suspend method

i2c-core: driver [cs42888] using legacy resume method

imx_3stack asoc driver

Initialize HDMI-audio failed. Load HDMI-video first!

ALSA device list:

  No soundcards found.

NET: Registered protocol family 26

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

Waiting for root device /dev/mmcblk0p2...

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new ultra high speed SDHC card at address aaaa

mmcblk0: mmc0:aaaa SS08G 7.40 GiB

mmcblk0: p1 p2 p3

EXT3-fs: barriers not enabled

kjournald starting. Commit interval 5 seconds

EXT3-fs (mmcblk0p2): using internal journal

EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode

VFS: Mounted root (ext3 filesystem) on device 179:2.

devtmpfs: mounted

Freeing init memory: 192K

INIT: version 2.88 booting

Starting udev

udevd[65]: starting version 182

Starting Bootlog daemon: bootlogd.

Configuring network interfaces... eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:00, irq=-1)

udhcpc (v1.21.1) started

Sending discover...

PHY: 1:00 - Link is Up - 100/Full

Sending discover...

Sending discover...

No lease, failing

Wed May 7 21:41:00 UTC 2014

INIT: Entering runlevel: 5

hwclock: can't open '/dev/misc/rtc': No such file or directory

Starting syslogd/klogd: done

Stopping Bootlog daemon: bootlogd.

Poky (Yocto Project Reference Distro) 1.5.1 webbg3flight /dev/ttymxc0

ラベル(2)
0 件の賞賛
返信
1 解決策
12,581件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
12,582件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
12,601件の閲覧回数
YixingKong
Senior Contributor IV

Robert

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信
12,601件の閲覧回数
RobertCorrellus
Contributor II

stopped the boot on both machines and examined the memory and found that u-boot had set-up the register.  So my issue is in the u-boot build.  Where are the snvs register values set in uboot?

EVK md command data:

Hit any key to stop autoboot:  0

=> md 0x020cc004

020cc004: 80002100 00000000 00000000 00000000    .!..............

Custom board:

=> md 0x020cc004

020cc004: 00000000 00000000 00000000 00000000    ................

0 件の賞賛
返信
12,601件の閲覧回数
YixingKong
Senior Contributor IV

Robert

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信
12,601件の閲覧回数
YixingKong
Senior Contributor IV

Robert

If your questions had been answered, please click Correct Answer/Helpful Answer, otherwise keep exchanging your words with assignee.

Thanks,

Yixing

0 件の賞賛
返信
12,601件の閲覧回数
JackLee1z
NXP Employee
NXP Employee

Hi Robert,

You need to blow SEC_CONFIG[0] in efuse to start RTC. Please refer to the following page for more details:

Q&amp;A: How to program i.MX6 eFUSE?

For i.MX6SL fusemap, please refer to reference manual, Chapter 5.

MX6Sl EVK U-Boot >  imxotp read 4

bit 1 represents SEC_CONFIG[0]

You can blow the bit and try again.

MX6Sl EVK U-Boot >  imxotp blow --force 4 0x2

BR,

Jack

0 件の賞賛
返信
12,601件の閲覧回数
YixingKong
Senior Contributor IV

Robert

I will try to find an AE to help in this issue.

Thanks,

Yixing

0 件の賞賛
返信
12,601件の閲覧回数
RobertCorrellus
Contributor II

I printed the evk rtc-snvs register in the rtc_set_time function.  I noticed that the NPSWA_EN bit for the SNVS_HPCOMR register is different.  Where in but boot/load process are these set?  This is the bit that allows non-privileged access to the SNVS registers.

EVK registers:

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0000 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0004 ----register value = 0x80002100

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0008 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x000c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0010 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0014 ----register value = 0x80000b00

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0018 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x001c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0020 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0024 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0028 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x002c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0030 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0034 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0038 ----register value = 0x00000021

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x003c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0040 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0044 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0048 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x004c ----register value = 0x40000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0050 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0054 ----register value = 0x0007cdd4

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0058 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x005c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0060 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0064 ----register value = 0x41736166

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0068 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x006c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0070 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0074 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0078 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x007c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0080 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0084 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0088 ----register value = 0x00000000

Custom board Values:

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0000 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0004 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0008 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x000c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0010 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0014 ----register value = 0x80000900

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0018 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x001c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0020 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0024 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0028 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x002c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0030 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0034 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0038 ----register value = 0x00000020

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x003c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0040 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0044 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0048 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x004c ----register value = 0x00000008

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0050 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0054 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0058 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x005c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0060 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0064 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0068 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x006c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0070 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0074 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0078 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x007c ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0080 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0084 ----register value = 0x00000000

RMC --- func:snvs_rtc_set_time  Registers Offset=>  0x0088 ----register value = 0x00000000

0 件の賞賛
返信
12,601件の閲覧回数
RobertCorrellus
Contributor II

no I have not resolved the issue.  It appears to be an issue with the rtc_snvs.c file

root@webbg3flight:~# /etc/init.d/hwclock.sh start                              

RMC --- func:snvs_rtc_open                                                     

RMC --- func:snvs_rtc_open exit                                                

RMC --- func:snvs_rtc_read_time                                                

RMC --- func:rtc_read_lp_counter                                               

RMC --- func:rtc_read_lp_counter exit                                          

RMC --- func:snvs_rtc_read_time exit                                           

RMC --- func:snvs_rtc_release                                                  

RMC --- func:snvs_rtc_release exit                                             

root@webbg3flight:~# /etc/init.d/hwclock.sh stop                               

RMC --- func:snvs_rtc_open                                                     

RMC --- func:snvs_rtc_open exit                                                

RMC --- func:snvs_rtc_set_time                                                 

RMC --- func:snvs_rtc_set_time  ret = 0                                        

RMC --- func:snvs_rtc_set_time  old_time = 0x0                                 

RMC --- func:snvs_rtc_set_time  lp_cr = 0x20                                   

RMC --- func:snvs_rtc_set_time  time1 = 28000   ioadr = c08e8054               

RMC --- func:snvs_rtc_set_time  time2 = 0x0   ioadr = 0xc08e8050              

RMC --- func:snvs_rtc_set_time  lp_cr = 0x21   ioadr = 0xc08e8038             

RMC --- func:snvs_rtc_set_time  ioaddr+LPCR = 0xc08e8038   mask = 0x1

0 件の賞賛
返信
12,601件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

rtc driver has been succesfully probed:

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

About the error message: this is related to Yocto. I would suggest you to report it to meta-fsl-arm mailing list.

0 件の賞賛
返信
12,601件の閲覧回数
YixingKong
Senior Contributor IV

Fabio

Could you keep working on this customer's issue please?

Thanks,

Yixing

0 件の賞賛
返信
12,601件の閲覧回数
RobertCorrellus
Contributor II

Added register writes to the SNVS register so the values are the same as the EVK board at the end of u-boot.

Not sure when or how the mx6slevk board sets these but this change in /board/freescale/custom_board/custom_board.c seem to allow a proper linux boot.

int board_early_init_f(void)

{

    setup_iomux_uart();

#ifdef CONFIG_SYS_USE_SPINOR

    setup_spinor();

#endif

    setup_rtc();     // RMC --- added function to set the snvs registers for rtc

    printf("     NOTE rmc: board_early_init_f \n");

    return 0;

}

void setup_rtc(void)

{

    u32 reg;

        reg = 0x80002100;

        writel(reg, SNVS_BASE_ADDR + SNVS_HPCOMR);

        reg = 0x80000b00;

        writel(reg, SNVS_BASE_ADDR + SNVS_HPSR);

        reg = 0x020cc038;

        writel(reg, SNVS_BASE_ADDR + SNVS_LPCR);

        reg = 0x40000000;

        writel(reg, SNVS_BASE_ADDR + SNVS_LPSR);

        reg = 0x020cc054;

        writel(reg, SNVS_BASE_ADDR + SNVS_LPSRTCLR);

}

0 件の賞賛
返信