Hi, Holger
You can wake up system from suspend via debug UART, RTC or keypad. I do NOT know what board and what kernel you are using, below are some example based on i.MX6Q SabreSD board with v3.0.35 kernel, for different board, the UART and RTC alarm still can work as wakeup source, but the sys interface path may be different. If you have other question, please tell me the board and the software version, I will give you a guide.
1. Wake up by debug UART:
echo enabled > /sys/devices/platform/imx-uart.0/tty/ttymxc0/power/wakeup;
Then click any key in debug console, system will wake up.
2. Wake up by RTC alarm:
echo +5 > /sys/class/rtc/rtc0/wakealarm;
system will wake up 5 second after suspend.
3. Just press power key(SW3) when system suspend to wake up it.